Machine Heat Recovery System - the igus heating concept with waste heat

We have been using 100% green electricity at our production site in Cologne since 2021. By replacing old injection moulding machines with new ones that are 40% more energy efficient, we've reduced electricity consumption by 11% in relation to increased production hours. We use gas to heat our production and office buildings. We switched to climate-neutral gas in 2021, but we were concerned that we were using resources for heating when enough heat was already being generated, namely at the injection moulding machines. And, as of 2023, we have around 800 of these, distributed over several buildings. How do we manage to use the waste heat? That's what a team of igus engineers asked themselves and started trying it out. The result: the concept for heating without gas by using the waste heat from the machines. The plan: to no longer heat any buildings at the company's Cologne site with gas and to make the concept freely available to engineers and mechanical engineers, i.e. to industry.

The idea

During the injection moulding process, the hydraulic motors of the injection moulding machines get heated. To prevent them from overheating, the motors are cooled with cooling water. The cooling water is provided by cooling towers, from which the cold water is pumped to the machines. There, the cooling water absorbs the waste heat from the motors and is heated and fed to the fan heater. A fan located on the fan heater heats the drawn-in air and thus heats the hall. At the same time, the heated cooling water cools down during this process and is pumped back to the cooling tower and the process begins again.

The system is variably adaptable and enables the assurance of constant temperatures even in particular production areas. It does not use the detour via a heat exchanger, which would lead to temperature losses. Additional heating of the water using compressors is also not necessary. Since heat is extracted from the hot water as it passes through the fan heater, the cooling requirement of the cooling tower also decreases, which in turn saves energy.
Schematic representation of the heating concept Schematic representation of the heating concept

Detailed view of the control unit Detailed view of the control unit

The control unit in detail


The device developed by our engineers sees to it that a fan heater within the production hall is supplied with maximum heat energy and at the same time prevents machines from being damaged by excessively high temperatures in the return flow. 
The heated cooling water from the machines enters the device via the inlet on the right-hand side of the device. Water flows through the electrically adjustable ball valve to a flow meter that measures the temperature. The temperature of the cooling water in this area must be at least the same as the desired room temperature so that the water can be routed to the fan heater via the dirt trap and the manual ball valve. Otherwise, the electric ball valve blocks the passage and opens the bypass via the electric ball valve. The water cools down as it passes through the fan heater. This temperature is recorded by the temperature sensor. The heat output of the fan can be calculated from the temperature difference and the flow, which is shown on the display. Since there is hot water inside the pipes, the device can be locked to avoid burns. Since there is always dirt in the return pipelines, a dirt trap is used to filter coarse particles. In order to replace this from time to time, the ball valve can be turned over manually. This will prevent any water from flowing back down from the fan heater and flooding the unit.

What happens next


The time between idea and implementation sometimes goes by in a flash, as was the case with our "hall heating" project. We performed tests and tried things out, and suddenly there was a breakthrough: we were working in T-shirts even though the gas was turned off. As of April 2023, we are in the process of adapting our concept so that we can offer it for free. We will talk about it at the 2023 Hannover Messe. If you would like to find out when and how you can benefit from our waste heat concept, subscribe to our newsletter or visit this page regularly.
 
Registration for the newsletter
Clipboard icon

More about igus


Plastics and sustainability

Small plant Plastic can be sustainable. We consider the sustainability of our products in three phases: during production, in use and at the end of the product's service life. Two aspects in particular have occupied us for years: CO2-neutral production and "zero plastic waste", i.e. having no waste in production. It is precisely here that many measures, some of them smaller, bring us closer to the big goal. 

Going into the future with curiosity

IMPS, the physical in-house trade show that can be experienced virtually Research in an area of 3,800m2, an open ear for customer ideas, and annual innovation presentations at our in-house trade show and at many trade shows worldwide ... all of this is what innovation means to us. We want to work with our customers to find new solutions more quickly. We keep an eye not only on the current problems, but also on the challenges of the future. Digitalization, for example, pervades all igus structures and is closely intertwined with innovation.

Virtual tour of the igus factory

Virtual tour of the igus factory Would you like to see the core of our business in Cologne from the inside? Immerse yourself in our 360° VR world, discover a wide variety of stations, and watch our employees at work. All stations are also accompanied by interesting information about the factory and machines. Come on in!



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH